Other Parts Discussed in Thread: INA139, OPA2317, OPA317
用OPA2317做的一个跟随器,如图片所示(R2接的是INA139的输出管脚),但是实测结果与仿真结果相差较大。实验测得:VP_1:0.160mV;VP_3:0.011mV,VP_4:0.1mV左右,VP_5:0.016mV,按照跟随器的原理,VP_1也应该为0.016mV左右啊,请问各位大神,是什么原因造成了这一种情况的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
实际的运放和理想运放之间的差异,实际的运放有偏置电压,偏置电流一类的非理想因素,导致输入为零的时候输出不为零。
根据PDF,OPA2317在+5V的电源下,输出失调电压最大也才为±100uV,偏置电流最大也才为400pA,根据实际电路折算成电压也就0.02mV左右。不应该有1MV左右。是否需要改为双电源供电??
OPA2317是轨至轨输入输出的,输入共模电压范围为(V-)-0.1V~(V+)+0.1V。
因此单电源供电没问题。