请问TI的工程师,AMS1200供电电源VDD1=VDD2=5V GND1=GND2=-5V。请问所谓的隔离,是不是可以在输入信号上存在一个4000V的信号一段时间<60s,而器件不损坏。然后保护电路可以在隔离时间期间(最少保护电路反应时间约几百ms)去切断该信号源通道,从而完全保护运放。如果这样不能,盼TI工程师推荐方案。该电路需要应用在信号输入失误导致后及电路损坏,期待你们的回答。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问TI的工程师,AMS1200供电电源VDD1=VDD2=5V GND1=GND2=-5V。请问所谓的隔离,是不是可以在输入信号上存在一个4000V的信号一段时间<60s,而器件不损坏。然后保护电路可以在隔离时间期间(最少保护电路反应时间约几百ms)去切断该信号源通道,从而完全保护运放。如果这样不能,盼TI工程师推荐方案。该电路需要应用在信号输入失误导致后及电路损坏,期待你们的回答。
AMC1200供电电源VDD1=VDD2=5V GND1=GND2=-5V
AMC1200的原边和负边单独的供电耐压是0-6V,不能VDD1=5V,GND1=-5V。供电压差不能超过5V。
隔离是指原边和负边的电压等级。比如原边DC500V,负边都是低压侧,可能只有24V。中间需要隔离,有工业等安规要求。不是你理解的这样使用的。
谢谢。
谢谢Amoeba的回答,的确是电源供电差最大6V,你说的原边DC500V是电源电压吧,如果500V即是隔离电压,那么存在以下问题
问题1:GND1是否应大于DC494V,如果该电压差大于6V时极可能导致器件损坏
问题2:VISO Insulation voltage per UL 高达4000V,这个是隔离电压,那为什么会有60s的承受时间,既然有,那么这个电压是瞬时电压,并非电源等级
问题3:这样的电压等级的场合真的存在吗?以上是关于电源供电的问题
问题4:输入共模信号的差值手册上是-250mv~+250mv.。是不是如果传感器故障,电压超过该范围,比如20V则无论时间长短极可能损坏
问题5:该芯片没有必要应用在同电压等级的电路吗?因为如果电源或者信号的输入范围超出规定范围都有可能损坏,那么也妨不了ESD咯