This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好。请问你的输入电压是多少,负载是多大?OPA551的最大电流不超过200mA,且当其|Vs|-|Vo|与其Io是有一定的关系的,可以参考figure3和figure4,即Io会随着|Vs|-|Vo|的增大而减小。
非常好的仿真,解释了上面原因!!!因为我需要最大输出5V电压,所以我用8V供电电压试验看下发热情况,另外需要的最大电流80mA。
非常感谢!
建议今后评估运放时使用TI的评估工具TINA-TI,方便,快捷,可靠性好。下载地址
当使用7.5V供电时,让OPA输出4.3V,电流输出100mA。工作过程发热量比较少,但是连续工作3分钟后,隔10秒钟左右会突然断掉输出电压Vout然后马上又有了输出,然后周期性这样重复下去,不知是如何原因。请麻烦指导下。非常感谢!
电路还是用的原来的?建议把反馈通路上的电阻和电容去掉。同时,如果输出端一定要驱动100nF的电容,建议在运放输出和电容之间接一个小电阻,可以先评估一下50 Ohm是否可行。输入信号的频率有多大?
您好!
还是按照上图接线,做实验时C29,C30都没接。把反馈电阻R42去掉后,输入电压与输出电压是严格的1:1。突然掉电及又突然有电不是OPA551的原因。是DCDC开关电源的原因,估计是因为买了假的LM2675吧,是市场上随便买的,看那芯片上的字符就觉得不是原装的。换掉开关电源后,OPA551工作完全正常。12V供电下发热也不大。
请问是否还需要接电容呢?
请问使用开关电源供电是否会对OPA551有影响?因为我准备是用LM2675给OPA551供电。谢谢
1. 反馈通路上的RC建议都去掉,从仿真发现这对RC并不能改善稳定性。输出端的电容是你的负载,这个电容是否要加,取决于你的应用,应用里有这样一个100nF的容性负载,则电路图里就加,否则去掉。如果输出端负载电容较大,建议在6号口和负载电容之间加一个小电阻10~100 Ohm来改善稳定性。此时电路的输出应该是电容C29的上板。
2. 如果应用场合对精度要求不高,可以试一下用DCDC供电,必竟运放都是有一定的电源抑制的。