Other Parts Discussed in Thread: THS3120
用THS3120做了一个简单的电路,按照理论来讲,其可以输出475mA的电流,然而我用其输出有效值7.5V的电压,带47欧姆负载,电流也就是160mA左右,芯片就发热了,猜不到三分子一的电流啊,请大家帮忙看看
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: THS3120
用THS3120做了一个简单的电路,按照理论来讲,其可以输出475mA的电流,然而我用其输出有效值7.5V的电压,带47欧姆负载,电流也就是160mA左右,芯片就发热了,猜不到三分子一的电流啊,请大家帮忙看看
你好。建议参照datasheet的figure47,去掉C1,且在输出管脚与R4之间添加一个50Ω的电阻,至于电流的话,建议对其输出电流要留足余量,不要满量程输出。
1. 我觉得你的测试条件不对,可以参照手册第4页表格,你可以发现475mA输出电流的测试条件是“+/-15V,RF=649 Ohm,RL=25 Ohm,G=2”。从你的电路看,你的G=5,明显不符合手册上的测试条件,所以没有得到475mA的输出电流是正常的。
2. 另外,7.5V有效值电压除以47 Ohm电阻,算出来的电流就是160mA左右,这没问题啊。
1. 输出到负载的功耗大约已经有1.2W了,且你的应用不仅是送电流,而是抽/送电流皆有,抽电流时会有过热的问题,建议试试看把电源电压降到5V,看看会不会有改善,如果没有改善,则建议加散热片。
2. 看上去你需要的·峰峰值有10V已经够了,建议换+/-5V供电,减小芯片的静态功耗。
按照475mA输出电流的测试条件是“+/-15V,RF=649 Ohm,RL=25 Ohm,G=2”设计电路,仍然在输出160mA的时候发热,我没有加散热片的原因么?
第一种电路第一级运放看到的负载是Rout+R2+R3||Rin,第二级看到的负载是Rout+Rin,一般Rout很小,所以第二级负载小,大电压下发热大。你第二级为什么不把负载挂在输出端?第二种电路负载基本上就是那个50 Ohm了,所以虽然电压没有放到最大,但是因为50 Ohm确实很小,所以输出到这个电阻上的功率大,第一级发热也就大。
另外需要输出多少电流取决于你的负载和输出电压,如果47 Ohm上一定要流过475mA,那输出电压的有效值就是大约22V了。感觉你的电路需要的应该是输出电压,而不是输出电流。