Other Parts Discussed in Thread: OP07, UA741
我用的+5V供电,输入1kHZ正弦波,输出的波形在波峰附近是可行的,但是其他位置都是一条直线,并且输出幅值也就六七百毫幅,我的电压跟随器没有接任何电阻,且同时更换了op07和ua741两种芯片,之前接了电阻但是输出波形都差不多。我在想是不是op07和ua741都是必须双电源供电的,不能只接电源和地。下面是我的电路图以及仿真
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这里有2个问题:
1. 首先,这两个运放都不是轨对轨运放,所以输入共模电压和输出电压都是不能到达供电电压的,你看看规格书就可以知道,在供电+-15V的情况下,输入共模最高也不能都在+-13~+-14V左右,必须留有1-2V的headroom。如果供电是地和+5V,那么其实真正的有效输入信号范围就很小了。假设等效为0-5V,那么实际有效的范围也就只有1-2V。
2. 从波形来看,输入波形是正负(如果你没用AC coupled),所有运放在单电源供电的情况下,输入正负,那么输入电压小于0(轨到轨)的时候,输出肯定是没办到达负值得,如果要使用单电源,同时输出跟随输入,必须在输入提供一个正电压偏置,一般在电源供电的一般。VCC/2。
谢谢。