Other Parts Discussed in Thread: THS3001, THS3091, BUF634
各位TI的工程师们,TI的高速运放作为后级输出驱动负载的芯片有很多,比如THS3091,THS3001,BUF634等等,从数据手册上看,THS3001的输出电流比较小,但是压摆率和供电范围很宽,如果用THS3001作为后级是不是需要2-4块并联才可以;THS3091看上去是这三个芯片里面指标和性能最好的,可是实际制作的时候,我用两级并联输出来驱动50Ω负载,效果并不是很好,它的增益平坦度在30Mhz以后会急剧下降,我的同学做出来的效果和我的差不多:BUF634可以算的上是真正的高速缓冲器了,但是它的压摆率远不及THS3091;所以,我现在有一个疑问,到底什么时候选择THS3091,什么时候选择BUF634。请各位工程师能够给我一些你们选型的经验,或者用过这两款芯片的感受。感激不尽