Other Parts Discussed in Thread: LOG114, TLE2037A, TLE2037A-Q1, OPA211
我想要找一个放大芯片,它既能对输入的信号中的直流(幅度有正负)放大也能对输入的交流(幅度有正负)放大,输入信号电平是微伏到毫伏,频率是DC到5MHz,信号时前端系统处理了的信号。可以有推荐一下那些芯片满足这些要求不?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LOG114, TLE2037A, TLE2037A-Q1, OPA211
我想要找一个放大芯片,它既能对输入的信号中的直流(幅度有正负)放大也能对输入的交流(幅度有正负)放大,输入信号电平是微伏到毫伏,频率是DC到5MHz,信号时前端系统处理了的信号。可以有推荐一下那些芯片满足这些要求不?
谢谢!
前一个帖子写的是nV到mV,这一个帖子写的是微伏uV到mV,应该以哪个为准?另外,你想把信号放大多少倍?或者说,放大到多大的幅度?
要是能转化成电流输入就好了,有log114之类的对数放大器。不过如果一定是电压输入的话,最好能说明
1. 明确的电压范围,到底是多少uV到多少mV
2. 预期要多大增益,或者说把这样一个电压范围的信号放大到多大范围
3. 后级是带ADC还是继续走模拟信号处理
另外建议不要一帖多发,一个主题开一个帖子讨论就足够了。
电压是10几uV到几百mV,放大倍数几十倍就可以了。
我前段时间也买过log114,我是单电源5V供电,我看那个pdf输入要压缩的电流一般都是光电二极管的反响电流,我选的是I1为参考电流,log114的输入的电流I2的幅度可以有正负啊?不是那个对数比为log(I1/I2)啊,I2输入可以是有正负的福度啊?这也是我一个有点疑惑的地方。
10uV到100mV,这个动态范围有80dB了。这么大动态范围,首选对数放大器。另外一般的运放也很难实现这种应用,offset电压低于10uV,很难做。建议对前端信号源做处理,把正负输出的电压信号转化成单极性的电流输出,然后用对数放大器处理,比如log114.
TLE2037A-Q1,优点是low offset/low noise/high BW。注意一下这个Q1,没有Q1的TLE2037A是军用产品,估计国内买不到;有Q1的汽车电子类产品,应该能买到。
OPA211,offset和noise性能稍差(但是也能满足你的应用了),优点是有TINA model,可以在软件里做仿真。
你这个应用,估计要用到两级运放。因为推荐的两颗运放带宽是45M和50M,如果放大10倍,即使用单极点近似,-3dB带宽也到5M了。如果考虑实际情况中引入的输出端极点,带宽会更低。所以把增益分开做,每级都别做太大,保证闭环增益在5M内平坦。