This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5630B异常,所有原理图来自官网5630-slau287a

Other Parts Discussed in Thread: LM317, TAS5630

异常现象:

1、按下reset开关后,LM317的电压被拉低到5V,再也恢复不了

2、SD脚对地电压为1.5V

  • 补充说明:reset开关按下后供电的LM317发热严重,reset脚无电压

  • 你好

    建议从下面开始分析

    1)在reset脚被拉低前,芯片是否工作正常?

    2)reset脚是高阻输入状态。如果是无电压检查下reset输入是否正常?

    3)断开LM317, 采用其他电源供12V,看下是否是LM317的问题。

  • 之前是否工作正常?

    reset开关后,器件被重置,在上电瞬间对电流有个很大要求,看下是否是功放过流保护了。

  • lm317没问题,通电未按下reset之前都工作正常,ready指示灯,双差分IC也工作正常。后来分析是不是2N7002内部带有二极管,D 、S两端不能反转用,正在试验中。还有调试时候可以先不上TAS5630的高压吗?

  • SZXX

          你好!

           经过查找,官网的reset电路是错误的,经过修正电路是能正常工作了,但装上散热器后就不知道为什么没有输出了,拆掉散热器后还是没有。现在测得:SD端电压为1.6V,READY端电压为0V。请问下,可能是什么原因引起的?

  • szxx

        你好!

        现模块正常工作,有波形输出,但有几个地方有疑问?

    一、reset电路有波形输出时,开关是连接到地的。请问:设计时候是不是初次要把开关连接到12V,以后就不用了;

    二、正常工作时候,shutdown指示灯常亮,此时SD端的电压为1.6V,好像不满足设计参数,还是指示电路有问题?

    三、clip指示灯正常工作时不亮,此时CLIP端的电压为1.8V。只有关掉电源后会闪一下

    四、输出滤波电感发热严重,基本参数是按照bom表要求的,是否还有什么其它特别要求。

    谢谢!!!