This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于THS7368和 OPA360的使用问题

Other Parts Discussed in Thread: THS7368, TVP5158, OPA360

我目前正在做的项目是这样的,需要传输6路模拟视频信号PAL(分辨率为720*576)制的,我们想在将模拟视频信号传输给TVP5158时进行模拟增强,即输入的是模拟信号,输出仍然为模拟信号。在网上查到了THS7368和OPA360,主要疑问是THS7368能否滤波放大六路模拟PAL制式的视频信号,因为THS7368里面我看到了6个接口,然后就是OPA360主要问题是是否可以对模拟视频信号进行增强,然后输出是否仍然为模拟PAL制信号。两款芯片哪个更适合我的情况或者还有没有更好的推荐,不知道TI公司有没有模拟增强亮度和对比度的芯片
  • THS7368 全高清滤波器和 6dB 增益的 6 通道视频放大器 凭这个介绍就可以认为应该能够满足你的要求;

    OPA360 为 3V 视频放大器, 也是这类应用的器件. 是否复合你的要求, 还得看包括信号带宽, 信号范围等等因素