HI,
1、公司产品用到了全差分放大器LMH5401,GBP达到了8G的放大器,在使用中发现带宽只有几十MHz
2、正好手上有LMH5401EVM 评估板,拿来测试了下,其带宽也就是20M左右,不知道到是不是测试方法不正确的原因?
3、测试条件:(使用带有50欧姆SMA的屏蔽线连接信号源到EVM板)
1>EVM使用单电源5V供电,焊接RB-,使V-接到GND
2>单端信号输入,20K,115mV,
3>差分探头测试输出,此时示波器显示为20K, 100mV
4>信号源幅度保持不变,逐渐增加信号源频率,等频率增大到13MHz的时候,示波器端信号幅度减小为70.7mV左右
5>根据100mV减小到70.7mV,约为-3dB衰减,估算信号通道带宽为13M
4、附上EVM资料连接,请大家发表下看法,谢谢!

EVM用户指南:www.ti.com.cn/.../slou401a.pdf
LMH5401 datesheet: www.ti.com.cn/.../lmh5401.pdf