您好,我最近做谐振放大器,谐振频率为15M,最后结果测出来-3dB点的频率范围为3M,远远不能达到指标,感觉是并联谐振的品质因素太差。查了一下资料,想要提高品质因素就把L增大C降低,可是由于电感的品种和精度没有电容高,所以我选择了固定电感,最后固定电感1uh,电容为100p左右可以达到谐振频率点,但我现在想提高品质因素,请问我必须增大L减小C还是可以通过其他途径来提高品质因数,希望可以得到一些系统的讲解,谢谢指点!
原理图如下:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我最近做谐振放大器,谐振频率为15M,最后结果测出来-3dB点的频率范围为3M,远远不能达到指标,感觉是并联谐振的品质因素太差。查了一下资料,想要提高品质因素就把L增大C降低,可是由于电感的品种和精度没有电容高,所以我选择了固定电感,最后固定电感1uh,电容为100p左右可以达到谐振频率点,但我现在想提高品质因素,请问我必须增大L减小C还是可以通过其他途径来提高品质因数,希望可以得到一些系统的讲解,谢谢指点!
原理图如下:
为什么要加R8,看上去R8会增加损耗,恶化你的品质因数啊。如果不加R8,谐振频率会怎样?品质因数?
开始没有加R8但是电路很容易自激,加上以后就好了,这样确实降低了选择性,但是考虑到稳定性我就加上了。我刚才把R8拿掉以后电路还是自激了,我再把R5,R7增大试试,谢谢
保证稳定震荡的情况下,把R9减小一些,看看效果怎么样。
我把R5加大,自激解决了,最后谐振频率为15.04M,-3dB的带宽为200K,已经满足要求了,但是我测得矩形系数只有5.6,看别人做的可以达到4点几的,如果要把矩形系数继续降低请问采取什么措施啊?至于R9,打算三级连起来以后先不接负载,后面加一级推挽式输出然后带负载效果或许会好一点。最后再次表示感谢!