我想请教一下,TI的OPA2209运算放大器,Datasheet上面写的是轨至轨运放,同相输入端 输入+10V,反向输入端输入-10V,输出是够能有20V。是否在4.5~36V的电源轨上,满足20V输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想请教一下,TI的OPA2209运算放大器,Datasheet上面写的是轨至轨运放,同相输入端 输入+10V,反向输入端输入-10V,输出是够能有20V。是否在4.5~36V的电源轨上,满足20V输出。
输出电压范围为(V-)+0.2~(V+)-0.2,当输入电压在4.5V~36V之间时,输出电压可以有20V输出。
如果是电压是 双电源供电 +15 和-15 能输出 20么?
输出电压的范围您不是看到了吗?V-=-15V,V+=15V,输出电压范围为-15.2V~+14.8V。
嗯。好的。有没有什么 差分信号转单端信号的运放推荐,输入是正负10V的,输出可以是20V;或者可以变0-10V。