This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADC模拟量信号输入前级处理问题

Other Parts Discussed in Thread: OPA454

输入模拟量信号如下,差分信号,0~10V,-10~+10V

我打算用一个运放进行差分转单端信号,Vout最高是20V或者-20,有什么运放满足这个要求,当输入-10~10,能输出20/-20。ADC支持单极性 正负20V信号。

另外一种思路,就是 ADC只是支持正负10V信号,在差分转单端的时候要对信号进行衰减一半,此时又有什么运放合适。

麻烦推荐一下下,或者提供其他思路。谢谢。