Other Parts Discussed in Thread: THS7372
原始信号来自镜头的YPBPR信号,采用AC耦合的方式(备注:直流耦合的时候,Y信号的负信号全部被截掉,后端图像无法显示),芯片采用5V电源供电,三路信号均采用0.1u电容隔直以及采用2M电阻上拉到5V。
有图像显示,但是图像亮度太大,偏移了正常显示;
问题1:为什么采用THS7372芯片后图像颜色会变化?
问题2:采用相同的隔直以及上拉电阻,为什么每一路level shift是不一样的,其中PB、PR上移1V左右,Y信号上移1.3V左右?