This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm2902差分放大的调零问题

Vin1和Vin2都输入0.5V时,Vout最低输出大约0.05V;

Vin1和Vin2都输入1V时,Vout最低输出大约0.1V;

Vin1和Vin2都输入3.3V时,Vout最低输出大约0.6V;

输出无法调零,最低输出可达0.6V左右,要求在5V范围内,最低输出在0.1V以内。

怎么调零?请求指点。