Other Parts Discussed in Thread: OPA2846, LF412
您好,我设计一个运放检波电路,想请教下这个电路中opa2846运放的相关问题。
检波的电路如下图,信号源的输入信号频率为600kHz,幅度值500mV
现在有以下几个问题:
1、同一个电路使用OPA2846进行检波的时候,仿真输出检波信号噪声峰峰值约为不到1mV,实际电路信号噪声峰峰值在200mV内;把该电路的运放换为LF412进行检波,仿真输出信号噪声峰峰值约为250mV,实际电路信号噪声峰峰值可达到1V左右;仿真波形图见下方,我想知道究竟是运放的什么参数对检波输出信号噪声峰峰值起到了作用?为什么OPA2846的检波效果就比较理想,其他的运放就不行呢?
2、实际电路中,OPA2846运放正负5V工作,芯片发热,大概45度左右,状态是否正常?
3、该电路在使用OPA2846检波的时候,输入信号固定,输出信号滤波前和滤波后都会出现幅度缓慢下降的情况,大概每秒0.1mV,持续下降,这个有办法解决呢?或者说我应该修改电路?怎样修改?
4、OPA2846运放的电源电流26mA左右,如果要达到OPA2846的效果,有没有其他低功耗的运放可推荐?
附图
1、使用OPA2846检波的输入信号和输出信号
2、使用OPA2846检波的输出信号放大
3、使用LF412进行检波的输入信号和输出信号
4、使用LF412进行检波的输出信号放大