如下图所示,依照芯片手册,设计了参数如下:R取2.7K,C取1.2pF,带宽75MHz,采用了光电二极管PIN S6063,TINA仿真带宽也足够,但做了PCB之后只有3MHz的带宽,希望各位指点一二
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 输出电压当然对的,不对的话估计是自激振荡了。
2. 50欧姆是用来做传输线阻抗匹配的。
我发现OPA657、OPA847这些器件都比较敏感,板子上的分布参数对设计影响很大。
我看了下示波器接口,有个13pF的电容到地,和50欧姆构成低通网络的话带宽也有1/(2*pi*R*C)=244.86MHz,不会限制带宽吧。还有您提到的“下面层没有进行掏空处理”,这个指的是芯片底下吗?如果我现在PIN产生的光电流是mA量级的,PIN管在反偏8.4V时结电容为4pF,我换了OPA847,反馈极点为74MHz,3dB带宽为104MHz,算出其他的电容电阻参数分别为0.29pF(手册上说surface-mount resistors have a parasitic capacitance of 0.2pF, 所以我就把PCB上反馈电容的焊盘悬空了),7453.15欧姆(焊接时采用7.5k),测出来就是我问题里描述的3MHz。