11
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
那个相位曲线就是用TINA仿真的结果,只不过稍加处理再显示出来。处理方式是,若相位<-180度则+360度(对于相角而言,+360度后等效于原相角),这样,最终使相位控制在+/-180度范围内。这个电路的相位曲线,正好在50Hz处穿过-180度,按照这个规则,将50Hz以后的相位一律+360度就得到上面的相位曲线。有些软件里会做这样的变换,可能TINA里面没有做这样的处理,因而显示效果不太一样,实际上结果是一样的。
噪声谱的问题,这个电路里噪声源很多,有些在负反馈环内,有些在环外。滤波器对于环内噪声源的频率响应和对于环外噪声源的响应完全是相反的。出现那样的形状一点也不奇怪。但要解释为甚么有个峰有个谷那就麻烦了,得推导出频率响应来。。。这么复杂的网络,您还是饶了我吧。大家都这么能推那还要仿真软件干嘛。