我想用双T型正弦波振荡电路产生100Hz、1kHz、和10kHz的正弦波,一直难调试出来,自激都比较难发生,而且大部分都是调试出正弦被切掉上下的顶部。开始考虑可能是运放不是轨到轨,可电源为正负5V,自激的被切掉的峰值只有4V左右,至今还不太清楚,求指教???双T型是通过高通和低通来滤出比较单一的正弦波,是不是理论的带通越窄就正弦波形越好?还有,有时匹配R11和R10时比例为68:10k,有时又是3k:10k,这个比例具体应多少为好?是不是有不同的类型???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 手册上并没有明确指出+/-5V供电下的输出摆幅,个人认为被切掉的峰应该是因为输出摆幅不足所致。
2. 324是一颗比较老的芯片,手册写得也很简略,评估起来不是很方便。建议你评估一下OPA171,这颗运放手册比较全,价格也比较便宜。
用OPA171搭了一个类似的双T型正弦波发生器,其中
1. 用一个阶跃的负电源模拟起始时刻;
2. 在双T网络中加入限幅的二极管,避免正反馈驱动运放输出碰到最大允许的输出电压轨。
1. 上电前电源电压引脚是悬空的,我们可以假定这时的电压时GND,或是其他电压。上电后,电源电压会固定在+/-5V上,相对于悬空状态说,电源电压实际上是经历了一个阶跃的过程,从悬空电压阶跃到+/-5V。
2. 起振后负电源稳定在-5V,阶跃只是用来模拟。
3. 正反馈比例没仔细研究,你可以看一下网上相关的资料。调电路的过程中发现增益太小的话起振后的波形是个衰减震荡。