Other Parts Discussed in Thread: OP07
看到有的设计中,运放(OP07)供电电源中串个小电阻,不知道有什么作用?有的在12V时串电阻1K。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应该一般还配有个电容,起到RC低通滤波的作用,同时对运放有个保护作用,可以限流,不过不要过大。
首先看手册第5页图14,可以发现这个电阻是用来调输入offset的。然后看手册第2页电路图,IN1和IN2在进入第一级电路后实现V->I的转换,通过在OFFSET N1和OFFSET N2脚连接电阻到VCC,可以调节IN1和IN2两条电流之路的电流值,从而抵消因为运放offset电压产生的误差电流。