Other Parts Discussed in Thread: MSP430G2553, TLV5638, THS3095
用msp430g2553和dac 做任意波形发生器时,
用TLV5638做发生源信号最大频率是多少?
条件: msp430 dco 16MHZ 与dac串行通信。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430G2553, TLV5638, THS3095
用msp430g2553和dac 做任意波形发生器时,
用TLV5638做发生源信号最大频率是多少?
条件: msp430 dco 16MHZ 与dac串行通信。
从手册第6页的表格来看,ts(FS)在fast mode下最快可以跑到1us,对应1MHz;考虑最坏情况时,可以跑到3us,对应大约330KHz。测试条件是RL=10KOhm,CL=100pF。当然,如果你的应用中RL和CL较小,应该可以再快一些,大致来看,最大频率应该在300KHz~1MHz。
AWG的话,DAC驱动能力不强,后级至少还需要加一级放大器,可以作为Buffer。
可以看看THS3095.
www.ti.com/product/ths3095