This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA551的UA和PA两种不同封装区别

请问TI公司,贵公司的OPA551UA 和OPA551PA在芯片设计时,是否是同样的设计方案。我实验室在购买了OPA551UA在自己设计的电路中没有实现功能,但是选择了OPA551PA封装芯片实现了功能。希望TI公司给予指导。谢谢。

  • 1. 从手册第二页的表格看,UA和PA的测试数据是相同的,不同的是封装方式,UA是SO-8,PA是DIP-8。

    2. 建议你确认一下芯片的来源是否是正规渠道。另外,如果一片UA无法实现功能,换几片其他的UA再试试看。

  • 你好,我可能买到了盗版的OPA551UA芯片,因为我在申请了贵公司的样片,通过万用表电阻档测量引脚关系。发现自己买的20个OPA551UA与样片不一样。昨天样片已到,能够实现功能。希望贵公司确认是否有一批次芯片不可以工作或者是其他的原因。因为我们这个项目如果批量生产估计需要1000多片吧。谢谢指导。

  • 1. 假冒的芯片可能根本不是OPA551UA,有可能是报废的芯片重新打上了TI的logo。TI生产的芯片出厂前都会送去测试,通过测试的芯片才能出厂。

    2. 建议联系正规代理商购买芯片。