This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

选一款可放大1MHz的输入电压幅值为10mVp-p左右的差动输入电压放大器

Other Parts Discussed in Thread: INA129, THS4151, THS4150, OPA211

您好,请您帮我选一款可对1MHz的输入电压幅值为10mVp-p左右的信号进行放大的差动输入电压放大器,预计信号要放大到3.5V左右,我想应该是要两级放大。而我的电路对响应时间要求很严,要进行频率跟踪,故要求放大器不能输出相对于输入有很大的相位滞后,请您帮忙选一款合适的放大器,谢谢。

我在ADI公司的官网上对所有放大器芯片进行仿真,结果发现有许多输出误差都大于1%,没有合适的产品。

  • 1. 你的电源是多少伏的?10mVpp的信号上有没有共模偏置?

    2. 怎样定义”输出误差“?输入一个10mVpp的阶跃信号,在一定时间(这个需要你提供)内,建立到1%以内?

  • 这个采样幅值电压10mV的正弦波交流信号 是通过1毫欧的采样电阻在输入电源电压在10~30V范围内可调时采样电阻上的电压,预计 也就十几至四十几mV,故需进行两级放大到大约3.5V左右,然后进行频率跟踪和后续处理。

    10mVpp的信号上有没有共模偏置? 这里电压应该差不多是20Vpp的交流正弦波信号,放大电路前级我采用差动放大,输出端有一隔直电容,故这里共模偏置可忽略。

    2. 怎样定义”输出误差“?输入一个10mVpp的阶跃信号,在一定时间(这个需要你提供)内,建立到1%以内?

    输出误差是指输出电压的实际值和放大器理想状态下的计算值(即设计增益下的实际值)之间的误差。

    输入差不多是一个20Vpp的交流正弦波小信号。

  • 这个采样幅值电压10mV的正弦波交流信号 是通过1毫欧的采样电阻在输入电源电压在10~30V范围内可调时采样电阻上的电压,预计 也就十几至四十几mV,故需进行两级放大到大约3.5V左右,然后进行频率跟踪和后续处理。

    10mVpp的信号上有没有共模偏置? 这里电压应该差不多是20Vpp的交流正弦波信号,放大电路前级我采用差动放大,输出端有一隔直电容,故这里共模偏置可忽略。

    2. 怎样定义”输出误差“?输入一个10mVpp的阶跃信号,在一定时间(这个需要你提供)内,建立到1%以内?

    输出误差是指输出电压的实际值和放大器理想状态下的计算值(即设计增益下的实际值)之间的误差。

    输入差不多是一个20Vpp的交流正弦波小信号。

  • 1. 输入信号是固定1MHz频率,还是频率可变的?如果固定1MHz,可以考虑INA129;如果频率可变,则TI的INA系列应该没有太合适的。原因是需要考虑到你的输入是30Vpp,也就是+/-15V的正弦波,在1MHz下,很少有运放能够覆盖这样一个输入范围。如果有办法把输入范围降下来,可能选择会多一点。

    2. 不过全差分放大器里倒是有THS4151和THS4150可供考虑,不过需要注意的是offset大了点,第一级和第二级之间要用交流耦合。

  • 发现THS也不行,因为THS用的时候要接成4电阻的反相放大模式,但是这四个电阻又会给输出信号源带来loading,所以也不行。现在纠结的问题是采样信号的频率对于INA来说还是有点高。这个频率是不是固定在1MHz附近?如果是个窄带的信号,那虽然INA带宽不够,但是可以人为造一个高的平带增益,使增益曲线掉到1MHz附近时还能有个10倍8倍,那INA129就可用了。

  • 发现还是要用4电阻的反相放大组态,附件里是仿真的TINA模型,噪声在750uVRMS,谐波失真0.2%,可将10mVpp输入信号放大到3.2Vpp。你可以用这个模型继续做优化。

    1MHz_10mV_2_stage.TSC
  • 因感应加热过程中负载的等效感抗是变化的,但变化不大,故频率是在1MHz附近小幅变动,也就900K~1100KHz左右摆动

  •       因感应加热过程中负载的等效感抗是变化的,但变化不大,故频率是在1MHz附近小幅变动,也就900K~1100KHz左右小范围内摆动,也就是说在加热过程中频率是在小范围内变化的。

       30V是主电路电源的电压,是固定的,不是指运放的输入电压;运放的输入电压预计是20Vpp~80Vpp左右的正弦波,偏置为0,运放的目的是通过两级放大把此电压放大到幅值为3.5V左右的正弦波信号,前级通过差动放大去除共模干扰,后级是一个反相放大使上述两级运放的输入和输出同相,请问什么样的放大器满足此要求,谢谢o(∩_∩)o

  • 已经在上个回复里把TINA仿真文件放在附件了,用的是两级OPA211,另附一份bmp文件做示意。