This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:TLV3501输出与SN74LV123A振荡器器的输出问题。

各位专家好:

我使用比较器TLV3501把模拟信号转化为数字信号,之后进入SN74LV123A振荡器,打算用比较器输出的数字信号的上升沿触发出两路稳定的数字信号。

SN74LV123A的R/C分别为1k和15pf。但是振荡出的信号总会有两个连续的波形。

具体图如下:

2为蓝色,是模拟信号。1为黄色,是比较器输出信号。4为绿色,是比较器上升沿触发振荡产生的信号。3为粉色,是4信号再次进入振荡器触发生成的信号。

图例,4信号就是比较器上升沿触发的信号,有两个波,本来应该只有一个。

分析原因可能是比较器输出的波形不干净,有振荡,导致后面的触发器以为有多个上升沿。所以多次触发。

请问,这个问题该怎么解决,是继续把比较器的输出信号弄干净?还是从触发器入手,防止因为输入信号振荡而多次触发?