Other Parts Discussed in Thread: PGA900
请问:PGA900的驱动只能安装道一台电脑吗? 我现在换了台电脑,PGA900EVM程序已正常安装,但是驱动按照操作装不上。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请您参考User's Guide来安装,您的电脑建议满足以下需求:
• Supported OS – Windows® XP, Windows 7 (32 bit, 64 bit)
• Recommended RAM memory – 4GB or higher
• Recommended CPU operating speed – 3.3 GHz or higher
User's Guide请参考这个链接:http://www.ti.com.cn/cn/lit/ug/sldu016a/sldu016a.pdf
PGA900GUI USER‘GUI DE 的第28页激活OWI有这么一段话
For OWI Activation
• Through I2C:
– The digital interface is enabled by writing 3 to MICRO_INTERFACE_CONTROL.
– The I2C communication parameters (speed, address length, and pullup speed) are set.
– The 3.3-V and 5.0-V power outputs are enabled.
– GPIO_OWI_ACT is set to LOW.
– GPIO_OWI_TX is set to HIGH.
但是如何设置GPIO_OWI_ACT 和GPIO_OWI_TX,是在评估板强行拉高/拉低?应该怎么操作?