This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV103H 不能正常工作

hi,

  手工做了一个DRV103H芯片的boom,原理图如附件图片所示,pin1接30k电阻,测得电压为2.29V;pin2和pin7为NC,电压为0;pin3接47k电阻,测得电压为1.24V;

pin4接GND(图片中未画);pin6接24V;出现的现象为: 当pin8=GND时,pin5-pin6间负载20k电阻 示波器测得50HZ的pwm,占空比差不多40%,之后改变pin3的电阻值没有任何作用;当pin8=5V时,pin5-pin6间一直为24V;

  请大牛指点,Thanks!