Other Parts Discussed in Thread: PGA112
我们现在想选一款PGA:
要求放大倍数是2的n次方,固定倍数输出,最大输出1000倍左右
双电源3.3V供电
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不知道你的频率要求,不过在低频领域,可以考虑PGA112。这颗芯片供电支持2.2V~5.5V,放大倍数支持1,2,4,8,16,32,64,128倍输出,可以把两个PGA112连在一起实现1024倍增益。