Other Parts Discussed in Thread: OPA1632
OPA1632用正负9V供电,增益约0.25,输入7V交流信号输出会失真吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA1632的输入共模电压范围为(V-)+1.5V~(V+)-1V,所以+-9V供电的话,能处理的输入信号范围为-7.5V~8V。
另外就是需要考虑GBW这个参数了。