Other Parts Discussed in Thread: ADS1262, CC2640
你好!我现在要设计一个电流检测设备,电流从0.1uA~300mA。设计思路如下:
1.电源必须用超低噪声LDO(5v to 3V或者 12V to 5V).
2.电流采样电阻采用2个温度系统好的电阻,例如用2个3 ohm +-0.1%,硬件根据放大器输出电压动态切换,电路是用一个还是2个电流采样电阻。
3.放大器输出后经过低通后送给ADC,然后用MCU采样这个ADC信号。
最近一直在找一个适合的运放,要求低失调输入电压,低输入偏置电流<10nA, 带宽(500KHz~1M),如果要准确检测非常小的电流,必须要考虑补偿放大器的Vos。麻烦您给出适合这个应用的运放和补偿的放大器的Vos方法,例如用DAC来补偿,如果有这方面的学习资料或者参考电路更好,非常期待你的回复,非常感谢!
另外如果要实现这个应用成本非常高,可以考虑测量电流从1uA~100mA,谢谢!