Other Parts Discussed in Thread: THS4304, ONET8531T, LMH6629, OPA656, OPA657, OPA847
将pin管的输出电流转换成电压,要求准确恢复直流、交流信号。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有更详细的性能指标要求吗?如果是找高速运放,可以考虑一下THS3404,LMH6702QML,THS4371,带宽都在1GHz以上,噪声和offset性能也都不错。
pin管的输入为光发射模块,速率为1.25G/b,要尽量不失真还原信号。
不太确定你的这个应用是不是要拿运放做。如果用运放,考虑一下THS4304(之前写错了),这颗运放带宽有3GHz,应该能够满足1.25G速率的信号要求。如果不用运放,建议把这个问题同时提到"接口时钟"版,看看那边的专家有没有什么好的方案提供给你。
如果是标准SFP光模块,输出的是数字信号。
接收Pin管后级,可以考虑一下TIA ONet8531T
www.ti.com/product/ONet8531T
你好,如果你是光纤通讯的话,那么ONET8531应该是可以使用在光纤接收端的。
如果没记错的话,光信号的消光比是等于逻辑"1"和逻辑“0”的平均功率之比。
你的1G信号难道是载波,要恢复1G信号上搭载的直流、交流信号?建议还是将具体的应用详细描述一下。
不太推荐直接用运放做,速率太高,直接用运放搭,问题太多。推荐专门用于光通信的TIA.带宽都大于1.25G。适合你的应用。
hi cheng, 首先消光比是测量发射侧的1和0的功率比,如果仅仅是为了测量消光比的话,不推荐使用这样简单搭电路来测量,因为你无法预测光路中的损失等,可考虑通过专用的示波器或者消光比测试仪来进行测量。