我是按照PDF上的电路设计的十倍同相放大器,可是上电后都出不了波形,而且还有自激产生,请问如何解决这问题啊?还请各位高手请教opa846的使用问题,我是为初学者....
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最好把电路图发上来,同时说明输入信号的直流,交流摆幅,频率,以及输出端挂的负载,以便进一步评估。
图就是PDF上的,输入100mv,10khz到10mhz~~~感觉都没opa690好用~~~
你是指手册第10页图1?
1. +/-5V供电是不是给对了
2. 如果源是个50Ω的输出,后级电路需要50欧姆匹配,则检查一下电路输入的输入输出匹配是否正确。
3. 输出端的负载电容有多大?
可以在反馈电阻上并个小电容,同时在输出端加个小电阻。具体的电路见附件,注意输出端的电容已经把你的负载电容包括进去了。
如果负载电容100pF,那么建议你在输出端再另外挂个100pF电容到地,这样可以把等效的电容做到200pF。