This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在我给同相输入端R30左端一个 6v 1.3khz的 正弦波信号,
在ADJ_R1和OPA_OUT1之间接一个10欧电阻。发现 OPA551很烫。
这是什么原因。这个由虚短虚断原理得知,
R37处的理想电流300ma(但是,在ADJ_R1和OPA_OUT1之间串一
个电流表 得到顶多95ma)请解答。
谢谢。此运放目的就是提供一个恒定的电流。
我如何调整电阻来获取一个能够输出90ma的电路呢?
你用错了。输出端和负输入端之间接一个10Ω的电阻,则电路是一个同相放大组态。此时由虚短的原理确实能推出R37处的理想电流是300mA,但是这部分电流是运放输出端提供的。从OPA551的手册第二页来看,运放最大的输出电流就只有200mA,没办法提供300mA这么大的电流,所以此时虚短的条件不满足,R37的电压肯定会被拉下来。
datasheet里面的200ma是最大直流,对交流来说应该是一个峰值。即交流的最大有效值也就是140ma。如果得到100ma的电流,输入峰峰值5v的1.3k交流信号,那么反相输入给予30欧 的电阻就可满足要求。请问这样理解对不对
如果输入峰峰值是5V,那么峰值就是2.5V,反相端30欧姆到地时,对应的峰值抽/灌电流是83mA,在+/-200mA以内,所以应该可以满足要求。