请教下OPA2335和OPA2375的输入阻抗是多少? 官方资料上没有说明,有没有ICL7650的 10的12次方么
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA2335是CMOS型输入运放,CMOS型输入运放的输入阻抗也很高,估计在Mohm左右,如果需要10的12次方的高输入阻抗,可以看下JFET型输入的运放。
OPA2375这个型号再确认下?
1M输入阻抗会不会太小了,放大mV级的信号会不会有干扰。OPA2277都有100M的阻抗。Jfet的有哪些输入失调电压为uV级的,同时输入阻抗较大的,谢谢了
你好,
即便是CMOS输入的放大器,输入阻抗(低频情况下不考虑输入端寄生电容)也会达到大几百M欧姆甚至G欧姆级。
如果想用JFET的放大器,你可以看下OPA192系列的放大器
Best regards,
Sulyn Zhang
那相对于 OPA2277 OPA2335 及您说的OPA192 那种芯片在性能上有一定的优势 或者说他们各自的优点 谢谢了
你好,
OPA192这个系列和OPA2277都是高压供电的可以支持到36V电压, 如果你系统需要高压供电需要考虑这两颗。先说OPA192和OPA2277,OPA192是TI新一代的放大器,它的DC(失调和温漂)和AC(带宽和压摆率)性能都要优于OPA2277;OPA2335是一颗零温漂低压低失调的放大器,供电电压小于5.5V,带宽比OPA2277略大比OPA192小,所以看你的应用要求了
如果回答了你的问题,请帮忙确认回复,谢谢!
Best regards,
Sulyn Zhang