Other Parts Discussed in Thread: THS3001, DAC2900
最终是要得到-6V~+6V范围内的40M单端信号。选用DAC2900差分电流输出2~20mA范围,接THS3001电流反馈型型单端输出放大器(该放大器+IN输入阻抗1.5MΩ,-IN输入阻抗15Ω),对具体实现有点懵逼,求高手指点!多谢啦~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最终的信号是通过SMA接口用同轴电缆接到相位调制器(一种电光学器件,且负载为50Ω)的SMA接口上进行光相位调制,
第一步:通过fpga控制DA输出40MHz频率、步进30mV的阶梯信号从-6V~+6V通过电缆连接到相位调制器扫描整个范围的电压;
第二步:然后找到对应的3个电压(比如-4.5V、0V、2V电压),然后还是以40MHz的频率随机给这3个电压通过电缆连接到相位调制器来进行相位调制(可能该时刻25ns输出-4.5V下一时刻25ns输出2V,这三个电压间的切换是随机的)。
看了THS3001datasheet正负端的输入阻抗分别1.5MΩ和15Ω,相差很大,不知道具体怎么设计电路,望指点。或者说推荐其他型号的放大器,能给参考电路就更好了