请教:
运放TL084采用正负电源供电,负电源的作用只是为了能输出0V(没有负电压输出),那么负电源的功耗很小,可不可以采用+12V,-5V这样不平衡的正负电源给TL084供电?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
@xyz549040622,
请教:您说的很麻烦是指什么,计划用TPS60403产生一个-5V电源,12-GND没办法保证0V输出。
谢谢!
@Kailyn ,
用TPS60403产生一个-5V电源可以不?
谢谢!
TPS60403属于电源类产品,建议您到“电源管理”版块下发帖。
如果手头上有TPS60403,产生-5V可以的,TPS60403的输出电流也足够,因为TL084不属于功放。电源芯片其他方面的专业知识就需要到电源版块咨询了。Gong Huang 说:@Kailyn ,
用TPS60403产生一个-5V电源可以不?
谢谢!