This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不建议这么做。6657的输入噪声在11nV/sqrtHz,最大的offset有7mV,直接放大100倍,输出端的噪声和offset没法接受的。如果只是1M的应用,没必要用这么快的op啊,OPA211或者OPA365应该足够满足你的要求了。两级放大应该不会出问题。
还是建议用两级。高速放大器里offset最小的都在0.4~0.5mV,如果直接用单级高速放大器,offset电压直接就把信号淹没了,为了恢复信号,你还要在输出端用交流耦合。同时,交流耦合时还要涉及到阻带截止频率不能太高,以免影响有用信号的放大。这一套流程比较麻烦,还不如用两颗单级运放来得方便。建议用OPA211,offset才0.05mV,就算直接放大100倍,输出端也就是5mV,不用交流耦合也可以接受。同时噪声低,带宽大,还是很适合你的应用的。