This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教:单级放大还是两级放大?

Other Parts Discussed in Thread: LMH6657, OPA211, OPA365

使用LMH6657做微弱信号的放大 需要放大100倍 信号带宽在1M 在datasheet中看到增益10时 3dB带宽在10M多的样子 若直接放大100 倍 带宽是否满足要求?若直接按照270M/100=2.7M 是满足1M带宽的要求 还是分两级放大保险?
  • 不建议这么做。6657的输入噪声在11nV/sqrtHz,最大的offset有7mV,直接放大100倍,输出端的噪声和offset没法接受的。如果只是1M的应用,没必要用这么快的op啊,OPA211或者OPA365应该足够满足你的要求了。两级放大应该不会出问题。

  • 请问你的信号是不是从直流到1M,如果是交流信号的话,可以采用一级放大。请问你的信号是从什么地方输出的阻抗是多少,幅是多少。选运放不只是要看带宽。

  • 是别人的一个传感器设计 现在我都推荐他们用TI的芯片 因为这个平台太给力了

    没有直流信号   输出阻抗在几十欧的样子  幅度从零点几毫伏到70毫伏

  • 还是建议用两级。高速放大器里offset最小的都在0.4~0.5mV,如果直接用单级高速放大器,offset电压直接就把信号淹没了,为了恢复信号,你还要在输出端用交流耦合。同时,交流耦合时还要涉及到阻带截止频率不能太高,以免影响有用信号的放大。这一套流程比较麻烦,还不如用两颗单级运放来得方便。建议用OPA211,offset才0.05mV,就算直接放大100倍,输出端也就是5mV,不用交流耦合也可以接受。同时噪声低,带宽大,还是很适合你的应用的。