Other Parts Discussed in Thread: AMC1200, AMC1301
采用AMC1200进行电流采样,如图片当VDD1和GND1没有供电,VDD2和GND25V供电时,VOUTP和VOUTN输出差值为2.5V左右?这是为什么呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
要注意AMC1200的差分输入电压典型值为250mV,最大值为320mV,固定增益=8,如果VINP – VINN=250mV的话,输出正好为2V,但是如果大于250mV的话,输出幅值就会大于2V,因此需要看下采样电流以及取的电阻值大小,或者VINP – VINN为多大。
我这边是VDD1和GND1没有供电的情况下 ,VINP 和VINN为悬空,只有VDD2和GND2供电的情况下,VOUTP和VOUTN输出差值为2.5V左右,我本来想是这种状态下VOUTP和VOUTN输出差值为0的。有没有这种功能的线性光耦推荐呢?
是的,我想可以做以下几种实验:
1)VDD1悬空不上电,只有VDD2上电的情况,比如固定5V或者3.3V,看输出情况。
2)VDD1悬空不上电,只有VDD2上电,并且是0~5.5V上升,看输出情况
2)VDD1开始上电,然后掉电,VDD2固定3.3V或5v上电,看输出情况-----这种情况我认为是输出饱和,比如最大320mV输入,增益为8,输出为2.52V。
你目前的这种情况,我想输出应该是0或者随机的。
实验1)2)做过的,VDD悬空不上电,只有VDD2上电5V,差分信号输出压差值为2.5v左右,可是我需要一款当VDD1悬空不上电,VDD2上电5V或3.3V时,差分信号输出压差值为0v的芯片,请问贵公司有没有类似的芯片呢?谢谢
可以看下AMC1301,这款隔离芯片集成了failsafe电路 ,当VDD1 power down,missing或者failure时,差分输出的是固定电平,压差值为0V。
可以看下datasheet 8.3.2 Fail-Safe Output部分的详细介绍。
不好意思,这个我需要再确认下,Figure47和Figure48主要是说明failsafe输出和clipping 输出 不一样。但是通过二者的波形可以看到,红色代表VOUTN,紫色代表VOUTP,从波形来看,二者绝对值差值几乎为0.