我知道6515是一款优秀的差分高速放大器,但是在我的应用中需要应对低频(甚至小于几十kHz)的输出情况。
下图是LMH6515手册给出的典型应用图,手册上说利用了下面的电感的馈点提高了输出摆幅甚至高于电源轨。但是在我的应用中还需要电感么?我应对的是低频和阻性负载的环境。
在LMH6515的评估版手册中也给出了参考评估版的电路,但是由于信号频率太低,使用变压器是不太现实的,询问一下具体的改造方法。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LMH6515输出需要加电感,LMH6517不需要,能否说下你的应用,对于这么低的频率,输出端1uH电感不够,可能需要提高电感大小。
40-200kHz 内的超声频段的信号接收和调理。 选择LMH6515 是因为手头正好有十片存货。如果不需要摆幅超出电源也是需要电感输出能量么?有没有改进的办法?感谢Kailyn的回复。
不好意思现在才回复,LMH6515输出建议通过加电感来设置共模电压,datasheet中也提到,如果给的供电电压范围比较宽,或者通过电阻方法来设置共模电压的话,则不需要加电感,但这种方法不推荐呢。Sontao Yang 说:40-200kHz 内的超声频段的信号接收和调理。 选择LMH6515 是因为手头正好有十片存货。如果不需要摆幅超出电源也是需要电感输出能量么?有没有改进的办法?感谢Kailyn的回复。
Although It is possible to use resistors and high voltage power supplies to set the output common mode, this operation is not recommended unless it
is necessary to DC couple the output.