Other Parts Discussed in Thread: TPA3255
使用TPA3255设计警报声放大器(输入信号为方波),电路参考官方dome板。
电源:48V;
输入信号:峰峰值3V, 频率500Hz;
目前输入正弦波,可以正常工作,单端输出36V正弦波。
但是,输入方波,占空比50%。立刻就会过流保护。
TPA3255,想问这款放大器是否合适输入方波?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.