最近用OPA2171AIDR(带宽3MHz)设计了一个2倍放大电路,放大器采用±5V双电源供电。输入信号是±1.2V的正弦交流信号。当输入信号频率为100kHz时,输出信号幅值正确,当输入信号频率大于150kHz时,输出信号幅值衰减,达不到2倍放大,且变为三角波形,请问这是OPA2171AIDR器件批次问题还是电路设计问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近用OPA2171AIDR(带宽3MHz)设计了一个2倍放大电路,放大器采用±5V双电源供电。输入信号是±1.2V的正弦交流信号。当输入信号频率为100kHz时,输出信号幅值正确,当输入信号频率大于150kHz时,输出信号幅值衰减,达不到2倍放大,且变为三角波形,请问这是OPA2171AIDR器件批次问题还是电路设计问题?
忘了说了,测试波形时已将C193、C194和C167焊掉不接,跟电容无关。
我计算了一下,当频率为150Khz时,需要的压摆率SR的大小:
SR=2*PAI*Vp*f=2*3.14*2.4*150*10^3=2.26V/us。
而实际OPA171的压摆率为1.5V/us,所以SR不够。