Other Parts Discussed in Thread: OPA4197
现象:上电后opa4197损坏,测量供电电源(+-15V)被拉低,取下opa4197,电源恢复正常。
说明:该电路是为了监测PVDD,PVEE电源的电压是否稳定(目前4路只用到2路),运放的输入取自这两个电源的负载端,输出经2K电阻分压后送到AD,读出该电压值,与DA设定值比较后做补偿。
1,VDD15,VEE15为opa4197的供电电源,+/-15V,来自隔离电源模块,驱动能力只有200ma,但电压很稳定。其他还有仪放,AD,运放用到这个电源。
2,PVDD_FB来自电源负载端的反馈,电压为4.6V
3,PVEE_FB来自电源负载端的反馈,电压为-3.9V
4,PVDD_FB1_HF、PVEE_FB1_HF为运放输出减半后送给AD。
求教这样设计电路有没有问题,为什么OP4197会损坏?比例还挺高,有十分之一的样子,
下边是AD部分电路