实验室做探究性应用,发现当VSP/VSN设置为+/-15V,VSOP/VSON设置为5V/0V,设置单端输出,VOCM直接从VSOP分压输入2.5V时,在增益为1或1/2下(其他未尝试),输出正弦波信号幅度峰峰值达到1.5V以后基本就会有饱和失真。
所以想请教一下,该芯片的输出信号幅度范围,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
实验室做探究性应用,发现当VSP/VSN设置为+/-15V,VSOP/VSON设置为5V/0V,设置单端输出,VOCM直接从VSOP分压输入2.5V时,在增益为1或1/2下(其他未尝试),输出正弦波信号幅度峰峰值达到1.5V以后基本就会有饱和失真。
所以想请教一下,该芯片的输出信号幅度范围,谢谢!
信号是怎样输入到PGA的?是不是直流工作点出了问题?比如进入PGA的信号不是个纯粹的交流信号,而是带着直流?最好能上传个电路图,以便进一步评估。
另外,可以测一个关键节点的电压,比如VCOM脚的直流是否是2.5V,VOP/VON的实际电压究竟是多少。还可以试着把输入信号频率降低,看看是否有改善。