Other Parts Discussed in Thread: OPA551, OPA552
TI工程师,你好!我看手册OPA552和OPA551的输出电流应该是一样的,但是我用OPA552正向放大VCC=30V,VEE=GND,接上150欧姆的电阻能输出200ma的电流,但是换成OPA551的话,接法都是一样的,输出电流最大只能到50ma,手册上说它两的输出电流一样是一样的吧!请问这是为什么呀 输出的都是直流。电路如图
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA551 和OPA552的区别在于OPA551是单位增益稳定,适用于低增益应用,而OPA552增益大于5稳定,在您的这个电路中,G=6,建议使用OPA552。
谢谢您的回答 麻烦您我还想问一下,现在OPA552总是缺货,国内很少从国外订货的话 时间太长了 ,TI有能替代OPA552的吗最好封装和线续是一样的,现在用的552封装是SOIC-8的,输出电流100MA以上带宽和压摆率倒是没多大要求,单电源供电,正向放大的就是VCC=+30V,VEE=GND,反向放大的就是VCC=GND,VEE=-30V。Kailyn Chen 说:OPA551 和OPA552的区别在于OPA551是单位增益稳定,适用于低增益应用,而OPA552增益大于5稳定,在您的这个电路中,G=6,建议使用OPA552。