在实际测试时,R26取4.7kΩ
电路如上图所示,当我输入端SUM电压为10V以下,对mos管的开关频率为160KHz,占空比为0.5时,电容C16上三角波的峰值电压相较于开关频率158KHz时会突然下降很多,表现出一个跳变的过程。当SUM<10V时都存在类似的突变现象,对应的开关频率逐渐降低;但是当SUM=11V时则没有这样的现象。这是为什么?如何解决?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 原因可能在于INA111的2,3号脚在SUM<10时差值变小。2,3脚的差值可以写作
Vdiff=(VCM+VDM)*R26/(R26+Rmos)=(SUM+VDM)*R26/(R26+Rmos)
当SUM变小时,Vdiff相应变小。等于说,要将2号脚抬升到原来的电压,需要更多的时间,从而开关频率降低了。
2. 另外,该电路在共模上有一个问题。因为INA111的Ref脚接地,所以Vo的共模是0,。但是OP07的3号脚接SUM,如果SUM不为0,那么OP07的2号脚共模电压也不会是0,从而电容C9会通过感应的方式向INA111的6号脚放电,维持电路的共模电压。是否需要这样?
3. 试试看把R26增大,看是否有改善。另外,可以试试看把SUM接到Ref去,保证两块芯片的共模是匹配的,然后再测一下是否还有原来的情况发生。也可以同时增大R26以及SUM和Ref接在一起。