This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA118的使用问题

Other Parts Discussed in Thread: INA118, INA282

您好!

我现在用INA118监测电流,电流大约几十个mA,CPU用的是STM32F103,电路图中的USD_curr直接接到CPU的A/D端子。

在上电后,输出脚就已经有大约0.85V的电压,动作时大约有1.1xxV,虽然电阻R521的压降有变化,但是INA118的输出几乎没有变化,固定在大约1.1,请教下文提出在哪里,多谢! 图中5V电压实际中已经修正为8V。

  • 另,2脚,3脚接续反过来仍然没有变化。

  • 2号脚和3号脚输入的绝对电压各是多少?是不是超出芯片的输入范围了?手册第2页有指出+/-15V供电下的输入范围,可以看到,并不是轨到轨输入的。另外R521下面的部分,电阻大约是多少?

  • 你好,谢谢回复。

    手册上述输入过压保护范围是±40V,我用的是30V。

    电路图是别人搞得,我刚才实测4脚不是-8,只有0.85V左右。

    如果不加VM,待机时候6脚输出有约0.88的电压,加上VM(30V)后,变成9V了。

    R521下面是motor驱动IC的桥式驱动电路的电源端,这个IC是ST的L6226.

  • 1. 4脚是电源脚,这个脚的供电不能错的。建议你先确定4脚电压确实是接到-8V,然后再做下一步的调试。

    2. VM这个电压高了。即使是+/-15V供电,输入的线性范围也只能到-13.9V~+14V(由手册第2页)。也就是说,如果你想芯片正常工作,+/-15V供电时,2脚和3脚的电压值要在13.9V~+14V这个范围内。从你的描述来看,VM=30V应该是过高了。

    3. 设法降低VM到(V-)+1.1~(V+)-1这个范围,如果不行,可以试试TI的电流并联监视器。比如INA19x,INA20x,INA282等。具体的选型网址

    www.ti.com.cn/.../parametricsearch.tsp

  • 您好!谢谢你的指导。

    1.-8V我从主板上跳线,现在大约是-7.70,8V的地方实际大约8.06.

    2.我的供电电压是8V/-7.7V,所以这个输入肯定是超过了。因为马达在15V以下无法启动,所以.....

     我会按照您的建议,考虑下别的片子。

    3.现在不大明白的就是,我把后端CPU拔去,在8V/-7.7供电时,输出会有一个电压,-1.45左右,当VM供电时,会有一个更高的正电压,10V左右,跟随VM的值增加而增加。而测流电阻两端几乎没有压降。

    应该说VM未加电时候应该不会有输出的啊。

  • 输出-1.45时候,输入端电压大约是-0.471。而加上VM后,输入端为16V左右,输出在9.6V左右。

  • 如果VM电压使INA118的2号,3号输入脚电压值不在(V-)+1.1~(V+)-1这个范围时,个人认为没有必要再做进一步测试了,因为这已经超出了芯片允许的线性输入范围,所以测出来的输出值没有什么实际价值。

    如果要单测INA118,建议把L2262关掉,然后在检测电阻下端串个电阻到地,调节电阻值使得流过检测电阻的电流是你先前预期的电流,然后保证VM的电压能够使2号脚和3号脚处在(V-)+1.1~(V+)-1这个范围,这样测出来的结果比较有参考价值。

    另外,注意到电路里只是检测了L2262 VSA和VSB的总电流,你不需要检测VBoot的电流?