Other Parts Discussed in Thread: INA149, INA139, ADS8472
输出的交流信号最大幅值是正负30V,峰值电流<1A。请问有没有合适的电流采集芯片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
需要隔离检测还是不隔离的?
不隔离的可以用高侧电流检测IC
隔离可以用霍尔,如果精度不高,开环霍尔也有IC,很小
目前电流检测芯片的共模电压我看了下,最低为-16V,宽共模电压范围的电流检测一般在-16V~80V。还没有低至-30V共模电压范围。
或者可以考虑高共模电压范围的仪表运放INA149。
我知道我的方案错在什么地方了。我一开始将交流电流认定不具有正负方向,因此选的是−2 V to +65 V共模电压电流检测芯片,认为正负30V的电压在这个共模范围内。
我用INA139+Rshunt的方案用TINA仿真一下看看。
另外顺便问一下:ADS8472这个ADC的采样率是可调的吧,通过那个CONVST脚。
下面是我以前写的分析帖子,其实我很想听听你的建议
http://www.deyisupport.com/question_answer/analog/data_converters/f/58/t/133837.aspx