This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1632发热

Other Parts Discussed in Thread: OPA1632, ADS1278, ADS1271

用OPA1632做ADS1278的差分输入,一上电OPA1632就发热,电路没问题,请问是什么原因,选用的封装是没有底部POWERPAD的OPA1632DR  SOIC封装

  • 请问热到什么程度?这个芯片的功耗确实比较大,发热是正常的,但是你所说的发热是什么程度?还有你是怎么验证电路是没问题的?怎么供电的?

  • 我找了个OPA1632,正负15V供电时,的确很热,就是功耗大的原因。如果你对功耗有要求,你可以考虑选用功耗低的运放。

  • 在正负15V供电时,静态电流测出来为14.7mA,跟datasheet中的指标一致,功耗确实大。

  • 试试OPA1632DGNR,MSOP-8封装,底部带POWERPAD。我有客户在用这个产品。需要样品可以联系我。jacky.han@welltechcom.com

  • 你好我的opa1632发烫,但还能工作,单会出现偏移。 这是输入0V时的波形。主要出现突变就会持续70个ads1271的采样时间大约1.4ms。以下是原理图:

  • 你关于OPA1632发热解决了吗?还有你测是有出现偏移吗,就是输入0V,但出现随机的突变。

x 出现错误。请重试或与管理员联系。