在使用OPA340的时候,我发现了一个很奇怪的现象,当我的OPA340 被接成电压跟随器的时候,调节2K的滑动变阻器大小,当运放整正输入端的电压小于1.43V左右时,运放发生错误,只能输出1.43V,当电压更低一点的时候,接近0.5V左右,运放直接输出VCC电压,该电压跟随器被工作在单电源5V。请问这是为什么呢?芯片上的印花是 第一行:BB OPA
第二行:340UA
第三行:38AZC
难道是假芯片?!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您买的芯片有问题,OPa340这款不管什么后缀,芯片表面marking为OPA340UA,而不是340UA。
建议通过TI授权代理商购买。