This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR115负载电阻

Other Parts Discussed in Thread: XTR115

如图,这个电路为12V直流供电。VCC5V是电源芯片输出的5V给传感器供电。Iout接个负载电阻RL到12VDC的负端。

有个问题,当压力在0pa时,负载电阻RL=50Ω,输出电流为4.11ma,更换RL=250Ω,输出电流为4.01ma,测量传感器的输出电压Vout一直都为0.2V,是什么原因引起负载电阻变化输出电流也变化?

  • 这是 三极管 Q1 的因素吧.

  •  更换Q1,BCP56还是一样的情况。XTR115的5脚电压也有变化,50Ω负载时比250Ω大一些,大概10几mv。RL=0Ω时,输出大概为4.2几ma。

  • 建议您参考一下这篇blog。问题的原因我觉得还是因为您把Iret直接接地的原因,您可以参考下这篇blog,里面详细介绍了哪些参考的是Iret,哪些电流流经Iret和Io。 

    https://e2e.ti.com/blogs_/b/precisionhub/archive/2014/12/09/part-2-two-wire-4-20-ma-transmitters-background-and-common-issues

  •  我看一下这篇blog,我的电路GND都是接在XTR115的3脚,和12V供电环路地没有接在一起,和这个资料、XTR115DATASHEET应该是一样的。如果接在一起,应该不会正常工作。按照XTR手册资料,这个负载电阻接不接,接多大阻值(不超过一定值,跟供电电源大小有关),在初始情况下,都应该为4ma,现在情况这个负载会引起输出电流的轻微变化。